a length unit of 'create_point_map_and_color_map' method in python
Posted: Tue Apr 12, 2022 12:49 pm
Hello,
I'm trying to get only the values on the z-axis using the 'create_point_map_and_color_map' method.
When I checked the stored values, I was curious about the unit of length such as 'mm' or 'm'.
maximum distance between camera and object(actually ground) is 12m.
but, stored values are from 8135.056 to 11.490.
Which unit of length is the correct? 'm' or 'mm' ?
thanks.
I'm trying to get only the values on the z-axis using the 'create_point_map_and_color_map' method.
When I checked the stored values, I was curious about the unit of length such as 'mm' or 'm'.
maximum distance between camera and object(actually ground) is 12m.
but, stored values are from 8135.056 to 11.490.
Which unit of length is the correct? 'm' or 'mm' ?
thanks.