Hello,
I'm working with libvisiontransfer in c++ for a vision project and have suddenly encountered an issue with my SceneScan Pro (monochrome). It has begun repeatedly disconnecting and then immediately attempting to reconnect, which has dropped the framerate to below 1fps. As a note, I am not using jumbo frames, but I am using a 5Gb/s ethernet to handle the increased volume.
I have attempted the following quick fixes:
Reboot the device, via unplugging and maintenance view of the web interface.
Connecting different ethernet cables (all tested to work at 5Gb/s) from the box to the switch I was using.
Connecting the device directly to my PC.
Visual check to ensure camera settings are identical between left and right cameras.
I would appreciate any assistance that can be provided on this issue. I'm completely stumped by this.
Repeated disconnection issue
Repeated disconnection issue
- Attachments
-
- settings.tgz
- Latest configuration from the SceneScan Pro.
- (166.67 KiB) Downloaded 916 times
Re: Repeated disconnection issue
Update to the issue:
After leaving the system off for a few hours and returning to it later, the device is now unable to connect to NVCOM or my c++ program. However, in the device's web interface, the preview framerate for the individual cameras and the disparity map have both returned to their normal 30fps.
After leaving the system off for a few hours and returning to it later, the device is now unable to connect to NVCOM or my c++ program. However, in the device's web interface, the preview framerate for the individual cameras and the disparity map have both returned to their normal 30fps.
-
- Posts: 123
- Joined: Mon Mar 25, 2019 1:12 pm
Re: Repeated disconnection issue
This seems to be a problem with the network connectivity. Very likely there is a high amount of packet loss on the network. This can be caused by the following:
- * A network interface with very little buffer memory (often found in laptops)
* A switch on the network that can't handle the high throughput and drops packets (we recommend the Netgear ProSafe line)
* Other high-bandwidth communication happening on the same 1-Gigabit link (e.g. 2 SceneScans)
* Low-quality Ethernet cables
Re: Repeated disconnection issue
Thank you for your quick response to my issue.
As of now, I've managed to fix the issue just by doing a factory reset of the SceneScan and re-uploading it's original settings. I am beginning to suspect that the issue was related to overheating from running the system continuously for too long a time during development and testing, as the issues have stopped entirely.
As of now, I've managed to fix the issue just by doing a factory reset of the SceneScan and re-uploading it's original settings. I am beginning to suspect that the issue was related to overheating from running the system continuously for too long a time during development and testing, as the issues have stopped entirely.
-
- Posts: 123
- Joined: Mon Mar 25, 2019 1:12 pm
Re: Repeated disconnection issue
We are currently not aware of any network issues in relation to thermal causes. Please let me know when you are experiencing similar problems again.