Search found 7 matches

by jay
Tue Apr 12, 2022 12:49 pm
Forum: Nerian Support Forum
Topic: a length unit of 'create_point_map_and_color_map' method in python
Replies: 1
Views: 7959

a length unit of 'create_point_map_and_color_map' method in python

Hello, I'm trying to get only the values ​​on the z-axis using the 'create_point_map_and_color_map' method. When I checked the stored values, I was curious about the unit of length such as 'mm' or 'm'. maximum distance between camera and object(actually ground) is 12m. but, stored values are from 81...
by jay
Mon Apr 11, 2022 2:33 pm
Forum: Nerian Support Forum
Topic: how to directly connect device with IP address in Python when device is not found
Replies: 2
Views: 7160

Re: how to directly connect device with IP address in Python when device is not found

as your direction, i installed 9.0.991 and find example code from 'example_pickle.py'

i should do develop many things, anyway i can save images now.

thanks for your help. and i will ask you many things before this project finish.

please. help me then.


thanks.
by jay
Mon Apr 11, 2022 12:53 pm
Forum: Nerian Support Forum
Topic: how to directly connect device with IP address in Python when device is not found
Replies: 2
Views: 7160

how to directly connect device with IP address in Python when device is not found

I downgraded a version of python and install wheel with pip. now, I have met another is issue. my PC do not find device information. last week, you give a direction to connect device with 'ip address' directly on visual studio(C++) ImageTransfer imageTransfer("192.168.10.10"); how do i con...
by jay
Mon Apr 11, 2022 1:01 am
Forum: Nerian Support Forum
Topic: how to use visiontransfer in python?
Replies: 2
Views: 6907

Re: how to use visiontransfer in python?

python version is 3.9.7 and processor is Intel i9-10900.

I will develop on pycharm.

should I downgrade a version of python?

Where can I find information about initial setup?

such as visual studio path and install wheel?

thanks.
by jay
Thu Apr 07, 2022 9:39 am
Forum: Nerian Support Forum
Topic: how to use visiontransfer in python?
Replies: 2
Views: 6907

how to use visiontransfer in python?

hello,

I am in a situation where I have to develop in Python.

I met this error message .

"ImportError: DLL load failed while importing visiontransfer"

what should i do?

thanks.
by jay
Sat Apr 02, 2022 3:55 pm
Forum: Nerian Support Forum
Topic: how to save color disparity map from 'ImageTransfer' ?
Replies: 4
Views: 11066

Re: how to save color disparity map from 'ImageTransfer' ?

thanks for quick reply. it is very helpful.
by jay
Sat Apr 02, 2022 1:36 pm
Forum: Nerian Support Forum
Topic: how to save color disparity map from 'ImageTransfer' ?
Replies: 4
Views: 11066

how to save color disparity map from 'ImageTransfer' ?

hello,

i'm trying to get color disparity map not NVCom but C++ code.

when i use a function 'writePgmFile()', i see '.pgm' images with gray-color.

and a result mat of 'toOpenCVImage()' function is 2-depth.

would you plz give directions to save color disparity map?

thanks.